AXIS#.JOG.DEC

Description

This keyword sets the deceleration ramp for jog moves.

Versions

Action Version Notes
Implemented 02-04-01-000  

General Information

Type Read/Write
Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

Linear: counts/s2, mm/s2, µm/s2, (custom units)/s2

See Acceleration Units for details.

Range Depends on units. See Acceleration Units for details.
Default Value

30,000 rpm/s

Depends on units. See Acceleration Units for details.

Data Type Float
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
AXIS1.JOG.DEC

501bh

02h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.JOG.DEC

511bh

02h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.JOG.DEC

6901

1AF5

Unsigned32

Read/Write

Acceleration

AXIS2.JOG.DEC

72437

11AF

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.JOG.DEC

6901

Float

Read/Write

Acceleration